This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA826: INA826 & XTR117 equivalents working at -55°C

Part Number: INA826
Other Parts Discussed in Thread: XTR117, , OPA192

Hello,

I am working on a design that is supposed to work from -55°C to +70°C and its storage temperature range is -60°C to +85°C.

I am using an INA826 as a bridge amplifier and the XTR117 for a current-loop.

But the INA826 is given to work from -50°C (instead of -55°C) and the XTR117 is given to be stored at the minimum of -55°C (instead of -60°C).

Does anyone know equivalents for those components which meet temperatures requirements ?

Thank you