Part Number: RCV420
Other Parts Discussed in Thread: TLV333
Tool/software:
Dear Team,
I'm designing a current to voltage converter. I'm having the attached one which was suggested by TI fellows but for now, I required few changes in the input as well as output
forum_5-9-24b_tlv333 - autosave 24-06-01 10_40 - autosave 24-07-08 14_04.TSC
the attached I-V converter having input current of 4-20mA and output voltage of 100mV-4.9v.
How can i achieve 1V output for 4mA and 4.9/5V for 20mA. 5V output voltage for 20mA input current is preferred.
Kindly check this and let me know.
Hoping to hear from you soon.
Thanks and Regards,
Mr. Prajwal P. Bhuse