Other Parts Discussed in Thread: LM339, , TLV1822
Tool/software:
Hello Technocrats,
We use the LM3932 as a comparator as follows,
Inverting comparator with hysteresis
Setting VA1 to 2.8V and VA2 to 2.54V


Adjust the input voltage of IN2- to 2.8V, then the output state changes, and oscillation is observed

I would like to ask if this phenomenon can be corrected, or are there any design parameters I need to pay attention to?
Thanks