Tool/software:
Hello All,
I have a system like 48V input and max 25A, if I use this circuit for this values is it okay?
https://www.ti.com/lit/an/sbaa353a/sbaa353a.pdf?ts=1729192792070
Regards

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello All,
I have a system like 48V input and max 25A, if I use this circuit for this values is it okay?
https://www.ti.com/lit/an/sbaa353a/sbaa353a.pdf?ts=1729192792070
Regards

Hello Oben,
The load is high side and the current sense is low side. +15V or +48V doesn't matter, unless the 1mili ohm resistor opens up. Then a larger Rg
25A is a 'large' 25mV input so the gain need to be lowered. If full ADC range is 27A; then gain should be 5V/0.027= 185.2, so increase both Rg to 690k/185.2 = 3.73k ; closest 1% is 3.74k
If 1mili ohm did open up, (48V - 5.6V) / 3.74k = 11.3mA; just over the ABS MAX input current. So if this is possible, go further.
(48V-5.6V) / 10mA = 4.24k ; so pick Rg bigger than that. Then pick Rf resistors based on what max current range to measure.
Hello Ron!
Thank you for your good feedback.
I made my voltage supply 3.3V for TLV333 and I made 1.5k Ohms resistors to 6.8k Ohms and when I calculated the max A is 32.52A.
What do you think about this is this works right?
Regards
Oben,
Checking fault current, (48V -3.3V - 0.6V) / 6.8k = 6.4mA input pin current (this flows to 3.3V bus that has to absorb this current); that is under 10mA. 3.3V / (690k/6.8k) = 32.52mV = 32.52A
690k is an odd value, 680k is far more popular. 3.3V / (680k/6.8k) = 32.52mV = 33A