This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help- PGA280

Other Parts Discussed in Thread: PGA280

I was going  through the data sheet of PGA280.  On page 15, Fig. 37, Fig. 38 and Fig. 39, the curves show that the output swings to 8 V. However, as per the test conditions on the top of that page, the VSON = 0 V and VSOP = 5 V. Does this mean that the output swings more than the power rails (in this case, more than VSOP) ?. In such a scenario, how can one use this for a 0-5V ADC ?. Do one need to clamp the output at 5 V with diodes ?.

Thanks,

-SM

  • I just noticed that this question had not been answered. Sorry about the delay.

    I believe that the curves reflect the fact that the output is fully differential and that VSON and VSOP go from 0V to 5V respectively.

    In the case of a swing of 8V, the swing goes from +4V to -4V.  At the most positive, VOP=4.5V and VON=0.5V; while at the most negative, VOP=0.5V and VON=4.5V. The VOCM is set to 2.5V.

    Joseph Wu

  • Thank you for the reply. That makes sense. It would be nice to have this information updated in the next release of documentation though.

     

  • No problem.

    I've passed your comment about the datasheet back to the development group.

    Joseph Wu