Other Parts Discussed in Thread: LMH6645, OPA604, OPA211, OPA1641, LM7171
Hi,
I would like to design constant ac current source with the following specifications:
output current (peak) = 1m-20mA
Frequency range = 1k -500kHz
Load = 10 ohm- 1000 ohm (resistive load)
I have followed the discussed topic on "constant ac current source" and from my understanding I designed ac current source based on advance howland current pump to meets the above requirements. From simulation I found that at frequency of 1kHz the output current achieved a bit higher than 10mA however the output current at 500kHz with 1000ohms load the output current is not as expected. Can anyone gives some advice on how to improve the situation? Does the problem comes from the bandwidth of LMH6645? I attached the circuits and the results I acheived.
Fazlul