Other Parts Discussed in Thread: INA138, INA216, INA210, INA270, INA199-Q1, INA225, INA226-Q1, INA220-Q1, INA190
Hi,
My customer requires follows;
・Sensing 0.085mA~8mA
・Requiring detection of no load(0mA)
・ADC is 10bit, VDD=3.5V.
I think that INA225-Q1 can achieve above requirement if Max. error[0.085mA] - Min. error[0mA] is larger than accuracy of ADC(3.42mV) as attached file.
Is my understanding correct?
Please let me know if you have any question.
Best Regards,
Kuramochi