This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi:
I have to design a 4-20 transmitter for a H9D-N3-2.5K-6B Zemic Load Cell. Datasheet here:
www.zemiceurope.com/.../H9D_Datasheet.pdf
In datasheet it states an Input Impedance of 700 Ohm, a Sensitivity of 3+0.008 [mv/V] (15mV Vfs for 5V excitation?) and combined Error of (+-0.023%). I'm trying to calculate the resistors Values.
1) Using equation 4 in figure 3 of XTR106 datasheet, i get a RLin of near 6Ohm. I think this is a bit low.. could it be right?
2) I use equations in figure 3 of XTR106 datasheet for calculating Rg, but it dependes of Vfs. However, i must add series resistance to the bridge cause it's input impedance is lower than 1K. In page 13 it says that this changes the bridges output... So Vfs changes? Should i calculate Rg with new Vfs modified by this series resistances? how to do that?
3)For calculating bridge balance, i need Vtrim... how does this value relates to my Load Cell?
Thanks!