Is there a trick to get the LM566 square wave output to oscillate at 50% duty cycle?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a trick to get the LM566 square wave output to oscillate at 50% duty cycle?
Hello Paul,
The LM566 is a discontinued device, so we can only offer very limited support.
The datasheet shows a typical duty cycle of 50%, so it is possible.
What supply voltage, frequency and control voltage range are you using? Split or single supply? Schematic? Do you have any scope photos?
One common mistake using these devices is attempting to "over-modulate" by using a large modulation index (trying to vary the frequency too much). 'Bending" the frequency too much can distort the output waveform. You should not try to deviate more than 10% if you want low distortion.
Also note there is a valid modulation input voltage range of 3/4 Vcc to Vcc for linear operation, so make sure your input voltage is within this range (may require level shifting).
Also see An-146, which uses the LM566 as a carrier current FM transmitter. Note the limited modulation range. It also shows how to tuse the LM566 in a single supply application.