Part Number: INA138
what will the Total Error % be with V(sense) at 3 mV?
- from Online Current sense amplifier error analysis INA138 with 3mOhm, 24Vdc: about 36.1% total error at 1 Amp load current. please explain the possibilities of total error population.
- 36.1% total error is the maximum?
- if I have a hundred (100) of INA138 parts tested for the same design, what can I expect? the total errors can be completely random numbers between 0 and 36.1%?
- from Figure 4. Total Output Error vs VIN in Datasheet: there is no trace data between 0mV and roughly 5mV of Vin. how to understand this region? for the same example above (Vin=3mV).