This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1863: L/R ch CMRR difference

Part Number: PCM1863
Other Parts Discussed in Thread: TAS5825M, TAS3251

Hi Team,

We found that PCM1863 2 Channel CMRR is some different (pin
30, Pi28/Pin29, 27) is connected to TAS5825M,

Have 2Pcs L/R within 1dB, but other 2Pcs PCM1863 L/R is 8dB just one is R Channel is relatively poor, the other L

Channel is worse,
So we A-B-A awap the PCM1863, and the characteristics changed after the test;
The Datasheet shows that the CMRR is 56dB. I would like to know what conditions were measured.

PCM1863.pdfTAS5825M.pdf At the same time, please help us to confirm if there are any suggestions for improvement of our line, thank you!