Other Parts Discussed in Thread: DAC38RF83
Hi,
Please tell me how to use this device and the following to solve the problem I am having with my customer's board.
LMK04821 is used for the following purposes.
DCLKout0: IQ modulator clock (84.384MHz, to FPGA)
SDCLKout1: SYSREF (2.637MHz, to FPGA)
DCLKout2: DACCLK (2025.216MHz, to DAC38RF83)
SDCLKout3: SYSREF (2.637MHz, to DAC38RF83)
Register settings are written in order from register 0
Finally, write 0x03 to Reg0x0139-> Used in Continuous SYSREF mode.
Confirmation details
Q1 : The register settings are written in order from address 0x00, but is there any problem?
Please let me know if there is a procedure.
·also,
Q2 : Is it possible to use it for SYSREF / DACCLK of DAC38RFxx in this mode?
When actually tried, spurious occurs near the 64QAM carrier. It disappears when this mode is stopped.
I don't know how the current continuous SYSREF was used.
The current SYSREF continuous use has spurious issues and should be avoided.
If we stop SYSREF continuous
I'm worried that "out of sync"-> "device will not be able to resync if out of sync".
(I'm sorry. I don't understand the operation of JESD204B well)
Q3 : Please tell me the recommended setting procedure when using this method.
Best regards,
Hiroshi