Part Number: LMK04610
I have a problem generating a single shot sysref from he lmk04610. I would like to use it in total bypass mode where we feed it with 491.2MHz on CLKIN0 and have it generate a single sysref (divide by 240) on outputs 3&4, and a divide by 4 (122.88MHz clock on clock out 5).
Depending on how we randomly click on TIC pro software i get two behaviors. Ether the sysref is a pulse train or it is not possible to trigger a sysref via a register write.
So I have a couple of basic questions
1: is there any requirement for either of the plls to be locked before sysref will work correcly?
2:Do you have a simulator for this pll , because TICs pro software lacks feedback as to what mode the device is in
Many thanks