Part Number: CDCEL913
Other Parts Discussed in Thread: CDCEL9XXPROGEVM
I saw in the datasheet (and in a previous Forum thread) that the "safe" number of EEPROM write cycles that may be performed is 1000; the same Forum thread mentioned that you can perform unlimited write cycles to the register RAM memory.
We are writing a software driver that will automatically write to the CDCEL913 registers every time our system powers up or resets. It is my understanding that if we set the EEPROM WRITE bit (Bit 0 of Byte 7) to "1" in our driver, then the register data will be written to the nonvolatile EEPROM memory every time the system resets; this process seems needlessly repetitive (since the EEPROM memory is nonvolatile), and we will exceed the 1000 "safe" write cycles fairly rapidly. But if we leave the EEPROM WRITE bit cleared "0"), then the driver will only write to the registers; we will basically be reconfiguring the CDCEL913 every time we power up our system, but since there is no limit to the number of register RAM writes that may be performed, this shouldn't be a problem.
Am I understanding this correctly?
Sean Heffernan