Part Number: LMK04832
Tool/software:
Hi,
I am trying to set up the dynamic digital delay for the LMK04832.
Section 8.1.9.5 Dynamic Digital Delay includes the following description:
"Dynamic phase adjustments of half a clock distribution cycle are possible by half step."
As mentioned in this description, I want to use the dynamic digital delay with half step. The target is CLKin0 and CLKin1, and I want to output the data after half-step delay from one of the CLKout pins.
Looking at the registers, it seems that the above operation can be performed in half steps with DCLKX_Y_HS (e.g., DCLK0_1_HS at 0x103).
On the other hand, section 8.3.4.2 Dynamic Digital Delay only describes a method for one clock step delay.
Additionally, this delay method seems to delay by the SYSREF or VCO clock. However, I do not fully understand the specific method, so it is unclear how to achieve the half-step delay.
Q1. Can this DCLKX_Y_HS be used for Dynamic Digital Delay?
Q2. Does this Dynamic Digital Delay perform the delay processing with SYSREF?
Q3. Please provide the setup time/hold time requirements for CLKin during Dynamic Digital Delay. Also, are these timing constraints relative to the sampling clock or to SYSREF?
Thanks,
Shunya