Part Number: CDCE949
Other Parts Discussed in Thread: LMK04832
Hello,
Two CDCE949 are connected in parallel and are fed by the same input clock (20 MHz).
What is the maximum Skew between a signal from the first devide and a signal from the second?
Please note that the first device will deliver 9 signals with 40MHz frequency and the second will deliver 3 signals with 40MHz and 2 signals with 20MHz frequency.
Best regards
Ahmed Fendri