Part Number: LMC555
Other Parts Discussed in Thread: TLC555, TLC556, SA556, NA556, SE556, NE556
The TLC555 shows dfferent output current capabilities, for source (10mA) and sink (100mA). The LMC55 show only one (100mA). Does this mean the LMC555 can source 100mA while the TLC555 can't?
Is the LMC555 a later design than the TLC555?
Will there be a LMC556 dual timer?
Finally a nit typo: the general layout shows a 0.001uF control pin capacitor. But all of the examples show 0.01uF