This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
the below schematic that is used to have an ON/OFF function is having a strange behavior as when the case is touched the ON/OFF function is operated from time to time without touching the button..The button is located on the metal box
W
What need to be checked/adjusted as apparently there is no glitch on the pin Thr/Trig?
thanks
Hello,
You can try adding a smaller (.1uF) supply bypass capacitor in parallel with the 47uF cap to help with high frequency noise. Is the button normally open, or normally closed? If normally closed, the capacitor C1 may be discharging when the metal case is touched which would put a low voltage on the Thr/Trig pins and trigger the timer.
Best,
Katlynne Jones
Hello,
The problem remains despite the bypass capacitor in // with the 47uF. The push button is normally open.
Thanks for your feedback
Hello,
Please also try adding a 0.1uF cap between the Trig/Thr pins and ground.
For clarification, is the timer circuit in the same metal case that the button is fixed to?
Is the metal case floating relative to the timer supplies?
Best,
Katlynne Jones
Hello,
The capacitor beetwen Trig/Thr do not improve the behavior. The timer is in the same metal case that the button is fixed to.The metal case is floating relative to the timer.
We do suspect that the parasitic capacitor beetwen the switch and his internal contact might be the issue.
Any recommendation there?
Thansk
Hello,
Hopefully that will work for you. I look forward to hearting the results.
Best,
Katlynne Jones