Part Number: LMK04828
Hi,
Can anyone clearly define the functionality of SYNC and SYSREF Divider in LMK04828
And how re-clocking SYNC pulse driven from Master LMK's SDCLKout makes slave LMK in sync with Master LMK's DCLKout ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04828
Hi,
Can anyone clearly define the functionality of SYNC and SYSREF Divider in LMK04828
And how re-clocking SYNC pulse driven from Master LMK's SDCLKout makes slave LMK in sync with Master LMK's DCLKout ?
Hello Shekhar,
The SYSREF divider divides the VCO frequency to create a SYSREF output frequency that acts as a common timing reference for multiple devices in a JESD204B system.
A further description of the SYNC/SYSREF feature of the LMK04828 can be found in section 9.3.1 and 9.3.2 of the LMK04828 data sheet. The following link as provides more insight into the SYNC/SYSREF functionalities: Understanding JESD204B Subclasses and Deterministic Latency
The LMK04828 SYSREF divider clocks a D flip-flop that accepts an input from CLKin0 or the SYNC pin with the proper mux settings. The output of this D flip-flop can be selected through the re-clocked mode of the SYSREF_MUX to drive the SYNC/SYSREF distribution path. When the reference input to the LMK is the same frequency as the output of the SYSREF divider which clocks D flip-flop, and the PLL is using a ZDM feedback clock at the same frequency as the output of the SYSREF divider, then a CLKin0 or SYNC signal meeting setup and hold times to the reference input can be used to perform (1) a deterministic divider reset and/or (2) re-clock SYSREF clock onto the SYSREF outputs of the LMK.
Section 5 in the following document will provide a further description on the re-clocking SYNC: Synchronization of Multiple LMK0482x Devices
Regards,
Kia Rahbar