Part Number: DP83869HM
Other Parts Discussed in Thread: DP83869EVM, DP83869
Hi,
I am using the DP83869HM in my design in media converter mode (Cooper to fiver 1000Base-T and 100Base-T). I would like to have my design review by an expert and provide their feedbacks. I am using TPS73525DRBT for the 2.5V (VDD2P5), the TPS73512DRBT for the 1.1V (VDD1P1), TPS73533DRBT for the 3.3V (VDDIO) to provide power to the devices.
The main goal is to use the component only with strap (We test with the DP83869EVM and it is working) without any microcontroller and so..
Can you please check if the configuration are good and if the power supplies capability are good for the component supplies ?
I have attached my schematic below: