When IC is interfaced with L&T Energy Meter, Meter_TX Signal is attaining 3.48V & -4.2V rather than reaching +5.5V & -5.5V levels. I'm attaching Scope Output for your reference as well as Energy Meter - MAX 3221 Schematic for your reference. Please provide clarification for this issue at the earliest. Awaiting for your reply.
Meter Side Picture for your Reference
1. Tx_Meter is connected to RIN of MAX3221
2. DTR is Connected to +V of MAX3221
3. Gnd is Connected to -V of MAX3221
Scope Output for Reference
Yellow Signal - METER_TX - 3.48V & -4.2V
Blue Signal - MCU_RX