FAQ: Logic and Voltage Translation > IxC
(CTRL + F) or (CMD + F) to search key words on this page!
Level Translation:
Buffers:
- [FAQ] What is a buffered LOW?
- [FAQ] What is the "VILC" Electrical Spec in I2C Buffers?
- [FAQ] What are the different I2C Buffer Direction Control Mechanisms?
- [FAQ] What connections of I2C Buffers are not Allowed?
- [FAQ] What Makes an I2C Buffer Hot-Swappable?
- [FAQ] What is Stuck Bus Recovery?
I2C IO Expanders:
- [FAQ] What is the Difference Between an I2C Device with the Family Name "PCA" and "TCA"?
- [FAQ] Can I2C IO Expanders be used in an Open-Drain Configuration?
- [FAQ] Can I Leave "..." Pin Floating on my I2C I/O Expander or I2C Switch (INT, RESET, PORT I/O, etc.)?
- [FAQ] What is the Auto Increment Feature in I2C IO Expanders?
- [FAQ] What are the Current Automotive Grade I2C IO Expanders?
- [FAQ] I2C IO Expander Schematic Checklist
- [FAQ] What are Sticky Registers?
Links to Helpful Application Notes:
Level Translation:
Buffers:
- Why, When, and How to use I2C Buffers
- Resolving Improper Implementation of the Static Voltage Offset on I2C Buffers (TCA9509 + TCA9517)
- I2C Solutions for Hot Swap Applications
- Maximum Clock Frequency of I2C Bus Using Repeaters (Buffers)
I/O Expanders:
- Features of TCAL Agile I/O Expanders
- How to Configure an I2C Push-Pull I/O Expander to Operate as Open Drain
- Implications of Slow or Floating CMOS Inputs