Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] IxC

FAQ: Logic and Voltage Translation >  IxC

(CTRL + F)  or (CMD + F) to search key words on this page!

Level Translation:

  1. [FAQ] How do the LSF translators work?
  2. [FAQ] What is PassFET Hangtime?

Buffers:

  1. [FAQ] What is a buffered LOW?
  2. [FAQ] What is the "VILC" Electrical Spec in I2C Buffers?
  3. [FAQ] What are the different I2C Buffer Direction Control Mechanisms?
  4. [FAQ] What connections of I2C Buffers are not Allowed?
  5. [FAQ] What Makes an I2C Buffer Hot-Swappable?
  6. [FAQ] What is Stuck Bus Recovery?

I2C IO Expanders:

  1. [FAQ] What is the Difference Between an I2C Device with the Family Name "PCA" and "TCA"?
  2. [FAQ] Can I2C IO Expanders be used in an Open-Drain Configuration?
  3. [FAQ] Can I Leave "..." Pin Floating on my I2C I/O Expander or I2C Switch (INT, RESET, PORT I/O, etc.)?
  4. [FAQ] What is the Auto Increment Feature in I2C IO Expanders?
  5. [FAQ] What are the Current Automotive Grade I2C IO Expanders?
  6. [FAQ] I2C IO Expander Schematic Checklist
  7. [FAQ] What are Sticky Registers?

Links to Helpful Application Notes:

Level Translation:
  1. PassFET Hang Time with TCA39306 I2C, I3C Level Translator
Buffers:
  1. Why, When, and How to use I2C Buffers
  2. Resolving Improper Implementation of the Static Voltage Offset on I2C Buffers (TCA9509 + TCA9517)
  3. I2C Solutions for Hot Swap Applications
  4. Maximum Clock Frequency of I2C Bus Using Repeaters (Buffers)
I/O Expanders:
  1. Features of TCAL Agile I/O Expanders
  2. How to Configure an I2C Push-Pull I/O Expander to Operate as Open Drain
  3. Implications of Slow or Floating CMOS Inputs
General:
  1. I2C Bus Pullup Resistor Calculation
  2. I2C Stuck Bus: Prevention and Workarounds
  3. I2C: What is the Auto Increment Feature?
  4. Understanding the I2C Bus
  5. A Basic Guide to I2C
  6. I2C Dynamic Addressing
  7. Choosing the Correct I2C Device for New Designs
  8. MSL Ratings and Reflow Profiles