Part Number: SN74HC595
Other Parts Discussed in Thread: SN74HCS595, SN74LVC3G34, SN74LVC3G17
Tool/software:
I am using SN74HC595DR in my design as a shift register, sometimes I can't get it, so I want to use SN74HC595DRG4 instead, but I find that it doesn't work and the signal doesn't output correctly, I don't see any functional difference between these two.
SN74HC595DR has normal waveform, the shift cycles is 8 cycles, the output is normal:

I replace U13 and U16 with SN74HC595DRG4, the output of U13 is zero(QA-QH), and the QH_(PIN9) has abnormal output, the shift cycles is 2, which is not normal either.


Can you give me guidance?Is the driving waveform of the chip correct? Why can't it output normally after replacing with DRG4?