This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74HC595: Logic forum

Part Number: SN74HC595
Other Parts Discussed in Thread: SN74HCS595, SN74LVC3G34, SN74LVC3G17

Tool/software:

I am using SN74HC595DR in my design as a shift register, sometimes I can't get it, so I want to use SN74HC595DRG4 instead, but I find that it doesn't work and the signal doesn't output correctly, I don't see any functional difference between these two.

SN74HC595DR has normal waveform, the shift cycles is 8 cycles, the output is normal:

I replace U13 and U16 with SN74HC595DRG4, the output of U13 is zero(QA-QH), and the QH_(PIN9) has abnormal output, the shift cycles is 2, which is not normal either.

I suspect there is a problem with the chip because the DRG4 chip I purchased does not have a logo on its surface, but I bought it from Mouser and I have asked this question on a forum before. The answer I received was that this is also normal. Later, I discovered that SN74HC595DR also has this type of chip without a logo

Can you give me guidance?Is the driving waveform of the chip correct? Why can't it output normally after replacing with DRG4?