Other Parts Discussed in Thread: TXU0204
Tool/software:
Hello,
we are using the level-shifter to transfer from 1,8V to 3,3V logical uart level. With our old controller, we had no problems regarding high Iq. now, after controller switch we got high Iq on the UART pins with high impedance imputs, where we propose different controller behaviour, but this maybe connected top linked thread.
to my question:
At the moment, we have OE tied to ground, setting the level shifter to always on. In the datasheet, OE can be set to high to disable the device. However, it was unclear, how much power needed to keep the device in the deactivated state, when e.g. a 100k pullup is used. The schematics are attached below.
regards