Other Parts Discussed in Thread: TXV0108, SN74AXC8T245, TXV0106
Tool/software:
Hi,
Our customer is considering SN74AVC32T245 for following voltage translation and data rates. Can SN74AVC32T245 accept them? Their system needs…
Tool/software:
Hi,
Our customer is considering SN74AVC32T245 for following voltage translation and data rates. Can SN74AVC32T245 accept them? Their system needs…
Tool/software:
Hi Team,
Will this circuit design work?
Tool/software:
Hi
In the previous product, the following was used:
SN74LV244APWR, 5V -> 3.3V Level shift …
Tool/software:
Hi Team,
I need S-parameter model for the SN74AXC8T245 part.
Tool/software:
Hi,
The SN54SLC8T245-SEP only shows the TYP data, does there have maximum data can share to us?
It seems better than SN74AXC8T245 but SN74AXC8T245 show minimum and…
Tool/software:
Hi Tier
My customer tend to use SN74AXC8T245 between ADS127L18 and a 3.3V MCU.
Could you help me check if SN74AXC8T245 data rate can support ADS127L18 communicate with…
Tool/software:
I have a question related to the DIR lines and minimum 1.4V. I need to translate to/from 0.7V and 1.8V logic and the datasheet is not clear if I can set the DIR lines…
Tool/software:
Can i replace SN74AXC8T245 with SN74LXC8T245.
The last one seems better / faster. I need to shift mostly up from 1V8 to…
Tool/software:
Is it possible for this device to switch the direction of pins 5-8 with a direction signal only during the read sequence of the QSPI interface?
I want to use it by controlling DIR1=Hihg and DIR2=Low in normal operation…
Tool/software:
Hi,
Our application as below,
Singal direction VCCB->VCCA
CH2: VCCA=0.66V
CH1: VCCB=1.2V
We found the signal has been distortion data rate about >10Mhz.
I need check…
Tool/software:
SN74AXC8T245PWR
Does this Buffer part support PWM signals transmission?
Tool/software:
So i need change the voltage LVL of a TDM 4mHz buss from 1v8 to 3v3. TDM master also changes ( it is either on the 1v8 side or…
Tool/software:
Hi there,
We bought 2 SN74AXC8T245 Evaluation Modules, but unfortunately the channel 1 of the 8 channels does not work for both EVMs.
We…
Hi,
I am using DP83TG720R-Q1 1000BASE-T1 Automotive Ethernet PHY. This will be connected to ZU-7 SoC from AMD. The I/O voltage supported by SoC…
I saw in the datasheet of SN74AXC8T245 that,“Simultaneous up and down translation is supported when both VCCA and VCCB are at least 1.40V.”.
I don't quite understand the specific meaning of "Simultaneous…
I found the SN74AXC8T245EVM Evaluation Module for bidirectional voltage translation. The datasheet shows it supports SN74LVC8T245 device. How can I order this?
Is…
Looking for a RAD hard part candidate to use as a level shifter between a 3.3V uP and a 5V output data. To be used in military or space environment, Similar to p/n SN74AXC8T245.
Hi,
I used GTL2014 and AXC8T845 from both direction level translator on adaptor board.
IO from silicon to port B of GTL2014 (vref 0.5V) with 71.5ohm PU resistor to 0.91V , port A (3.3V) of GTL2014 direct connect to port A (1.2V…
Hello,
I'm looking at the SN74AXC8T245 and SN74AXC4T774. Where in the datasheet can I find the drive current capacity for each output pin? I took a quick look, but was having trouble…
Is there a mechanical drawing available showing size of each part of the EVM board?
Hi
Does TI have 1.8V to 0.5V level shift? Data rate need abobe 20Mhz.
We use 74AXC8T245 but it only support to minimum 0.65V.
Thanks!
Jeff
Can I use the product with part number TXB0108 for CAN bus? When I look at the data rate of the material, it appears to be 100Mbps. Can bus is maximum speed 2Mbps. In this case…
We use SN74AXC8T245 to translate RGMII signals.
Port B link to PHY IC, VCCB is 1.8V.
Port A link to FPGA, the Bank voltage is 1.2V, so VCCA link to 1.2V.
Ethernet input is 1GHz…
Hi Team,
Could you pls recommend a device for ULPI? The data rate requirement is 60MHz@VCCI=1.2V. It seems the data rate drops as VCC drops.
Regards,
Hailiang
I designed a circuit using the Telit GE190C1-EUX GSM modem. Since the GSM side operates at a 1V8 voltage level and my processor operates at a 3V3 level, I used the SN74AXCH8T245…