Other Parts Discussed in Thread: UCC44273
Tool/software:
We are using SN74LVC1G17 with supply voltage of 3.3V, output external resistor of 10-ohm and capacitive load of 1.5nF.
the switching frequency is 500Khz.
the component Max…
Tool/software:
We are using SN74LVC1G17 with supply voltage of 3.3V, output external resistor of 10-ohm and capacitive load of 1.5nF.
the switching frequency is 500Khz.
the component Max…
Tool/software:
Hello,
Is it possible to power a door of the SN74LVC1G17 type at 1V8 and is its input compatible with 3V3?
In the datasheet it is noted:
• Wide operating voltage range…
Tool/software:
Hi Ti Team,
Greetings!
We like to know the Junction to Case (bottom) thermal resistance, Max Allowed junction temperature and Case Temp (°C) Max of SN74LVC1G17DCKR
Tool/software:
HI team,
When Vcc=3V, how much current can be output in what condition? Because there is two values in datasheet. Customer need 15mA, so if 16mA is in specific condition, there are no margin.
Regards,
Hayashi
…Tool/software:
Hi,
Please mention the max Junction temperature for the below part numbers.
SN74LVC1G17MDCKREP |
SN74LVC1G17DCKR |
TPD4S012DRYR |
HDC3022DEJT |
HDC3022DEJR |
REF35125QDBVR |
Regards,
Rama Krishna.
Tool/software:
Hello,
I am using the 74LVC1G17GV,125 buffer.
When i turn off the supply voltage, the output is disconnected from the input and rails? can i put 3.3V at the output when the VCC is 0V? i will not raise the VCC with…
Tool/software:
Hi,
we are survey n-and gate,supply voltage as below, we have choosing SN74LVC1G00 but seem 1.8Vin can't higher than SN74LVC1G00 VIH=2V.
…Tool/software:
Can you confirm the orientation of pin1 quadrant for SN74LVC1G17DCK3? This is not listed on page 18 of the datasheet.
Tool/software:
Hi Team,
My customer Inovance is evaluating SN74LVC1G17DCKR. They use the VCC=5V and there lack the spec of VOH when VCC=5V, as shown in below picture.
Could you kindly provide that what's the value of VOH in the…
Tool/software:
Hi TI Technical Support Team,
I am designing a PCB which will be used to count/measure the frequency. The measured frequency will be…
Tool/software:
Hello experts,
May I ask, what is the part number of SN74LVC1G17DBVR, but as a inverting device?
My customer is currently designing with SN74LVC1G17DBVR…
Tool/software:
Hi, this question is not specifically about the part number stated above, but more of understanding Schmidt Trigger. I read this application note and saw this statement highlighted in yellow.
May I know in which…
Tool/software:
Hi,
The input of my Schmitt Trigger is between 3.3V and GND, however, the datasheet only shows 3V and 4.5V. May I know how to get the exact values for 3.3V for both V+ and V- (min and max) threshold values?
Tool/software:
We are in need of information on the UBM (Under Ball Metallization)/SRO (Solder Resist Opening) of this device SN74LVC1G17YZVR
We need this for our DFM team to define their own land pattern.
Thank you,
Austin…
Tool/software:
Hi,
I want to ask about the input current for SN74LVC1G17DCKR.
It is written in the datasheet that the input current, A, needs to be a maximum of 5µ A. However, I have trouble finding any reference design…
Tool/software:
Dear Specialists,
My customer is considering SN74LVC1G17 and has a question about Behavioral SPICE Model.
I would be grateful if you could advise.
---
I would like to confirm whether the Behavioral SPICE Model of…
Tool/software:
Dear Specialists,
My customer is considering SN74LVC1G17 and has a question about Behavioral SPICE Model.
I would be grateful if you could advise.
---
I would like to confirm whether the Behavioral SPICE Model of…
Tool/software:
Can we get the min/typ package height for LVC1G17DPWR? ePOD shows 0.4mm(max), but no tolerance, min, typ value provided. Customer is asking for this. Thank you.
Tool/software:
Logic Team,
My customer is asking what “(7, N)” denotes in below table of the datasheet. Could you clarify?
Best regards,
Kojima
Tool/software:
Hi Team,
May I know if my SN74LVC1G17 VCC voltage is 3.3V, input voltage is 1.8V, will the output voltage is 1.8V or 3.3V?
And another question that if VCC is 1.8V, input voltage is 3.3V, output voltage will be…
Tool/software:
Hello,
I have a customer who ordered P/N:
They mentioned when they received the part, it had markings "C175, instead of "TA".…
Tool/software:
One of my customers is considering using SN74LVC1G17 for their new products.
At this moment, they have the following questions.
Could you please give me your reply?
Q1.
What is the minimum voltage of VOH and the…
Tool/software:
Dear All,
I've a question regarding maximum input voltage of SN74LVC1G17: if the component in supplied with 3.3V, is it possible to provide 5V on its input?
Thanks in advace for reply.
Kind Regards
Stefano
…Tool/software:
Hello experts,
My customer hopes to use SN74LVC1G17, however because they are designing 1 standardized board for several different models of refrigerator, for some models, they hope to keep the input floating.
…Tool/software:
Hello
How about the different between SN74LVC1G17DCKT and SN74LVC1G17DCKR ?
Are their performance the same?
Thanks a lot!
Bincheng zhang
ElectroCraft ZH