Other Parts Discussed in Thread: SN74AXC1T45
Tool/software:
Hello , I did go through TI website to search for SN74LVC2T45 PSPICE model but not available. Can you suggest any equivalent MPN that I can use as replacement for my…
Tool/software:
Hello , I did go through TI website to search for SN74LVC2T45 PSPICE model but not available. Can you suggest any equivalent MPN that I can use as replacement for my…
Tool/software:
Hi
What is your recommended complementary device to SN74LVC125A when shifting signals back to 3.6Vdoamin from 1.8V domain?
Br
Tool/software:
When we tested this IC, output waveform is sometimes oscillated. Would you see attached file?
In our application, pull-up/down register is not same condition.
This is not meet to the datasheet. Is this affected…
Tool/software:
Hello TI Team!
I'd like to know what is the meaning of the marking on top of the component SN74LVC2T45DCUR I'm working with.
More specifically I have two batches of boards. One is mounted with component…
Tool/software:
Hi Tier
My customer has recently received two types of samples, as shown, and their silkscreen and packaging look different, why and which is right?
Tool/software:
Thank you for your assistance.
We are currently undergoing a 4M change process.
We will need a data sheet comparing the old and new versions, so we would appreciate…
Tool/software:
Hello,
The block diagram of this device looks like it has internal buffers, but I don't see any other references in the datasheet. Does it have buffering capabilities? If not, are there any similar devices that…
Tool/software:
Hello,
Unlike other 74LVCxx products, SN74LVC2T45 current consumption is only is specifified when VI=Vcci or GND but not when Vi=5.5V.
Do you have any information on this subject?
Best Regards.
Sylvain
Tool/software:
皆さん、こんにちは。
2つのIC間で動作自由空気温度に違いがあると理解しています。
SN74LVC2T45-Q1を-40から+85の間で使用した場合、スイッチング特性(ポートAからポートBへの遅延時間など)はSN74LVC2T45と同じですか?
ありがとうございます
Tool/software:
Dear team,
We are using SN74AXCH8T245RHLR in our design,We need to know the maximum IO toggling speed of the mentioned chip.Kindly support.
Thanks & Regards,
Blessing…
Tool/software:
Could you help suggest products that can replace NLSX4373DR2G. and need p2p ,Thanks
Tool/software:
What is the actual Operating free-air temperature (T.A)? On the datasheet (SCES818B), it reads -40degC to 85degC, which is the same as SN74LVC2T45. However, I thought…
Tool/software:
Hello,
SN74LVC2T45's Datasheet says "This device is designed for glitch free power sequencing without any supply sequencing requirements such as ramp order or ramp rate…
Recent PCN has the SN74LVC2T45DCTR changing terminal finish from NiPdAu to Sn. Pure tin is prohibited in my application. Is there a version that would "only" come with NiPdAu?
We are plannig to use this buffer SN74AVC16T245 to control the different LEDs.
8 bicolor LEDs will sink 20mA current each from buffer SN74AVC16T245.
And for…
Dear Madam and Sirs,
follow question:
We will use the SN74LVC2T45 device as a clock driver mit 3,3 V Vcc and 20 MHz clock rate.
But in your datasheets I can't find no value or specification…
你好,TI专家,
SN74LVC2T45的datasheet中的10.1中要求“first power-up the input supply”,请问这里的input supply是VCCA还是VCCB?还是与DIR的值有关?
Team,
Can we consider that the propagation delays of falling transitions are the same between both component lanes (1 and 2)?
Or is there a significant gap?
Same question for the propagation…
We are using the SN74LVC2T45YZPR part in a battery design and have noticed that our current draw is sensitive to light exposure. We believe we have tracked this issue down to the SN74LVC2T45 parts.
Looking through the forum topics…
Hi there,
Based on the datasheet, the above part is a GREEN product, however the TI Label we received has no G1 reflected on the label.
Can you help to confirm or provide any document regarding this matter?
Thank you.
Hi Team,
Have a nice day!
Our device power supply is 1.8V and host output is 3.3V, therefore need to use level shifter…
Hello,
I am designing a FMC board for the communication between two main boards. The FMC board will be connected to both master and slave boards and two FMC will be connected through…
Hi,
I am using the sn74lvc2t45 to translate from 1.8V to 3.3V a ASP/I2S interface. The ASP_BCLK runs at 12.228 MHz. I am able to see a proper translation for all the ASP signals except the ASP_BLCK. The ASP_BCLK comes out but at…
Hi team,
What is the difference between SN74LVC2T45 and SN74LXC2T45?
Best regards,
Shunsuke Yamamoto
Hello sir,
May I ask the peak output current of SN74LVC2G17-Q1 when VCC=3.3V? and What's the maximum frequency of input signal and its duty cycle which SN74LVC2G17-Q1 can accept?
Best regards,
Wenting