Other Parts Discussed in Thread: TXU0304, SN74LVC1G125, TXS0104E
Tool/software:
Hi,
I have a design which uses three SPI slaves - two operating at 3.3V and one at 5V. The processor which is the bus master is 3.3V.
I was thinking…
Tool/software:
Hi,
I have a design which uses three SPI slaves - two operating at 3.3V and one at 5V. The processor which is the bus master is 3.3V.
I was thinking…
Tool/software:
Hi,
Currently, we have a footprint of TXS0104EPWR part in our existing design. Due to a design error, we have connected VCCA to 3V3 and VCCB to 1V8 in the design. Since TXS0104EPWR has the condition of VCCA ≤ VCCB…
Tool/software:
Hi,
Can you please explain what is mentioned in the datasheet P19, which states it can be either OD or push-pull? Could you clarify this? The driving capability of OD is determined by 10K/VCC, but how can it also…
Tool/software:
Team,
I want to know the terminal length of TXS0104ERUTR described below.
Would you tell me the dimension?
I also want to know whether the dimension can be used for any other products using the same package or not…
Tool/software:
Hey Team,
In the circuit we utilized for one of our industrial sensor read kits, we incorporated a TXB device as a bidirectional buffer. According to the datasheet…
Tool/software:
HI,
We are using Bidirectional Voltage translator for programming of PCIE Clock generator through I2C. But VOH,VOL of the FPGA is not matching with VIH and VIL of the translator. Is there any other similar translator…
Tool/software:
Hi team,
customer use TXB0104 for 5V to 3.3V level shift. The input signal is from optocoupler encoder and it's a open drain signal. I know that TXB0104…
Tool/software:
Hi TI supporter,
I'm designing my board ( red box), the I2C of U4 in my board working at 3V3 domain.
I'm adding the U3 as an translator to change from I2C_1V8 to I2C_3V3.
I wonder if it works or not. ( in controller…
Tool/software:
Hi Team,
I'm using the part TXS0104EYZTR in my design.
The OE pin should be referenced to VCCA only or VCCB also
Whether it is okay to provide VCC_1V8 power directly to OE pin.
Regards,
Manikandan R
Tool/software:
Hi expert,
Customer used TXS0104E for MDC&MDIO. So far the communication is no problem but some of the Vih and Vil measurement over the DS spec.
Do you see any concern about the Vih, Vil measurement result or it…
Tool/software:
Hi team,
as describe in the datasheet, is it mean that the Max data rate only support 2Mps under Open drain?
If not, what does this mean?
Also, may I know why is it only able to achieve 2Mpcs using open drain?
Tool/software:
Good afternoon;
our team is currently interfacing the TXS0104E-Q1 with SN65MLVD203B LVDS transceiver.
The challenge is the input threshold for…
Tool/software:
Hi Team,
We are using the Level translator IC TXS0104EYZTR, we are facing one issue.
without clock pulse on 1.8V side, 3.3V side we are getting clock (not pulse) high 3.3V.
Our doubt is whether we need give pull…
Tool/software:
Hi Team,
We are using the Level translator IC TXS0104EYZTR, we are facing one issue.
without clock in 1.8V side, 3.3V side we are getting clock high 3.3V.
Regards,
Sathya Priya N
Tool/software:
Dear Team,
In the above highlighted circuit, the USB VBUS is detecting and level shifting to 1.8V using n-Channel MOSFET. Can you…