Other Parts Discussed in Thread: SYSCONFIG
Hi,
I am designing a proof of concept using early samples of MSPM0L1306. It uses 4 PWMs to drive the windings of a motor. 4 PWMs are configured in the same way, with the exception of one generating interrupts for the control laws.
The project uses Sysconfig for the MCU configuration.
When I run the code, there are no signals coming out of one of the PWM pair (TIMG1). All other PWMs work as expected.
The Sysconfig file is as follows :
/**
* These arguments were used when this file was generated. They will be automatically applied on subsequent loads
* via the GUI or CLI. Run CLI with '--help' for additional information on how to override these arguments.
* @cliArgs --device "MSPM0L130X" --package "VQFN-24(RGE)" --part "Default" --product "mspm0_sdk@0.57.00.00"
* @versions {"tool":"1.15.0+2826"}
*/
/**
* Import the modules used in this configuration.
*/
const Board = scripting.addModule("/ti/driverlib/Board");
const GPIO = scripting.addModule("/ti/driverlib/GPIO", {}, false);
const GPIO1 = GPIO.addInstance();
const PWM = scripting.addModule("/ti/driverlib/PWM", {}, false);
const PWM1 = PWM.addInstance();
const PWM2 = PWM.addInstance();
const PWM3 = PWM.addInstance();
const PWM4 = PWM.addInstance();
const SYSCTL = scripting.addModule("/ti/driverlib/SYSCTL");
const UART = scripting.addModule("/ti/driverlib/UART", {}, false);
const UART1 = UART.addInstance();
/**
* Write custom configuration values to the imported modules.
*/
Board.peripheral.$assign = "DEBUGSS";
Board.peripheral.swclkPin.$assign = "PA20";
Board.peripheral.swdioPin.$assign = "PA19";
GPIO1.$name = "SUPERVISION";
GPIO1.associatedPins.create(2);
GPIO1.associatedPins[0].$name = "OUT_ENABLE";
GPIO1.associatedPins[0].pin.$assign = "PA15";
GPIO1.associatedPins[1].direction = "INPUT";
GPIO1.associatedPins[1].$name = "NFAULT";
GPIO1.associatedPins[1].internalResistor = "PULL_UP";
PWM1.$name = "MOTA_PH1";
PWM1.timerCount = 781;
PWM1.timerStartTimer = true;
PWM1.interrupts = ["ZERO_EVENT"];
PWM1.peripheral.$assign = "TIMG1";
PWM1.peripheral.ccp0Pin.$assign = "PA0";
PWM1.peripheral.ccp1Pin.$assign = "PA1";
PWM1.PWM_CHANNEL_0.$name = "ti_driverlib_pwm_PWMTimerCC0";
PWM1.PWM_CHANNEL_0.ccValue = 780;
PWM1.PWM_CHANNEL_1.$name = "ti_driverlib_pwm_PWMTimerCC1";
PWM1.PWM_CHANNEL_1.ccValue = 780;
PWM2.$name = "MOTA_PH2";
PWM2.timerStartTimer = true;
PWM2.timerCount = 781;
PWM2.peripheral.ccp0Pin.$assign = "PA23";
PWM2.peripheral.ccp1Pin.$assign = "PA24/OPA0.IN0-";
PWM2.PWM_CHANNEL_0.$name = "ti_driverlib_pwm_PWMTimerCC2";
PWM2.PWM_CHANNEL_0.ccValue = 780;
PWM2.PWM_CHANNEL_1.$name = "ti_driverlib_pwm_PWMTimerCC3";
PWM2.PWM_CHANNEL_1.ccValue = 780;
PWM3.$name = "MOTB_PH1";
PWM3.timerStartTimer = true;
PWM3.timerCount = 781;
PWM3.peripheral.ccp0Pin.$assign = "PA3";
PWM3.peripheral.ccp1Pin.$assign = "PA4";
PWM3.PWM_CHANNEL_0.$name = "ti_driverlib_pwm_PWMTimerCC4";
PWM3.PWM_CHANNEL_0.ccValue = 780;
PWM3.PWM_CHANNEL_1.$name = "ti_driverlib_pwm_PWMTimerCC5";
PWM3.PWM_CHANNEL_1.ccValue = 780;
PWM4.$name = "MOTB_PH2";
PWM4.timerStartTimer = true;
PWM4.timerCount = 781;
PWM4.peripheral.ccp0Pin.$assign = "PA10";
PWM4.peripheral.ccp1Pin.$assign = "PA11";
PWM4.PWM_CHANNEL_0.$name = "ti_driverlib_pwm_PWMTimerCC6";
PWM4.PWM_CHANNEL_0.ccValue = 780;
PWM4.PWM_CHANNEL_1.$name = "ti_driverlib_pwm_PWMTimerCC7";
PWM4.PWM_CHANNEL_1.ccValue = 780;
SYSCTL.peripheral.$assign = "SYSCTL";
UART1.enabledInterrupts = ["RX"];
UART1.$name = "MyUART";
UART1.peripheral.rxPin.$assign = "PA22";
UART1.peripheral.txPin.$assign = "PA21";
/**
* Pinmux solution for unlocked pins/peripherals. This ensures that minor changes to the automatic solver in a future
* version of the tool will not impact the pinmux you originally saw. These lines can be completely deleted in order to
* re-solve from scratch.
*/
GPIO1.associatedPins[1].pin.$suggestSolution = "PA2";
PWM2.peripheral.$suggestSolution = "TIMG0";
PWM3.peripheral.$suggestSolution = "TIMG2";
PWM4.peripheral.$suggestSolution = "TIMG4";
UART1.peripheral.$suggestSolution = "UART0";
Surprisingly, the TIMG1 is not present in the pinmux section at the end, which would explain why. However, its absence is strange, and adding it manually by editing the sysconfig fil in text mode doesn't solve the issue.
Sysconfig doesn't indicate any conflict on the pin attribution, and the function highlighted in the device representation is correct.
Any idea why this PWM has no output ?
Thanks in advance,
Best regards,
Adrien