Part Number: MSPM0L1306
Other Parts Discussed in Thread: SYSCONFIG
hello, I'm using MSPM0L1306 to generate a 38KHz pwm, I'm using the Resourse Explorer examples. I changed the "timer clock prescaler" to 84 and the "PWM Period Count" to 10 in the .syscfg file so that the "Calculated PWM Frequency (Hz)" is 38KHz. But I didn't get the 38kHz outputs... from 16KHz the output doesn't respond... Below 16KHz it's ok.