This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TRM describes that the AM243x supports 10 Mbps with RGMII on CPSW3G.
AM64x/AM243x Technical Reference Manual (Rev. H)
12.2.1.4.6.10.3 RGMII Interface
12.2.1.4.6.10.3.1 Features
"Supports 1000/100/10 Mbps speed"
Are there any requirements for PHY to be used at 10 Mbps with RGMII on CPSW3G?
For use at 10 Mbps with RGMII on CPSW3G, is it required to use in-band mode and a PHY that supports in-band status?
AM64x/AM243x Technical Reference Manual (Rev. H)
12.2.1.4.6.10.3 RGMII Interface
12.2.1.4.6.10.3.3 In-Band Mode of Operation
Does TMDS243EVM with DP83867IR support 10 Mbps with RGMII on CPSW3G?
If so, could you please tell me how to operate TMDS243EVM at 10 Mbps with RGMII on CPSW3G using the latest MCU+ SDK 09.00.00.35?
Best regards,
Daisuke
Hi Daisuke Maeda,
Apologies for delayed response.Yes, In band mode is needed for 10 Mbps RGMII.
To operate on 10 Mbps RGMII mode, make the following change in "EnetApp_initLinkArgs" function in your project:
Change as shown below:
After this, rebuild your project. Please let me know if you face any issues with the same.
Regards,
Shaunak
Hi Shaunak-san,
Thank you for your reply.
Could you also answer the rest of my questions?
Are there any requirements for PHY to be used at 10 Mbps with RGMII on CPSW3G?
For use at 10 Mbps with RGMII on CPSW3G, is it required to use in-band mode and a PHY that supports in-band status?
Best regards,
Daisuke
Hi Shaunak-san,
I do not have EVM handy, so I cannot check it right away.
I found a post that tried the change "EnetApp_initLinkArgs" but had an issue.
e2e.ti.com/.../am243x-cpsw-10mbps-packet-transmission-error
You said let me try and reproduce it locally.
I would appreciate it if you could try it with other examples or with the latest MCU+ SDK 09.00.00.35.
Best regards,
Daisuke
Hi Daisuke-san,
Yes, In band mode is required for 10 Mbps RGMII to work. I'll leave a couple of references down here if you want to read more about it:
The other issue reported with 10 Mbps UDP communication is being looked into right now. I'll keep you posted on the same after some internal testing. I'll get back to you by early next week.
Regards.
Shaunak
Hi Shaunak-san,
Thank you for your reply.
How to modify the code to set the EXT_EN bit in the CPSW_PN_MAC_CONTROL_REG_k register?
In the MCU+ SDK, "CSL_CPGMAC_SL_enableExtControl()" in csl_cpgmac_sl.c is provided to set the EXT_EN bit in the CPSW_PN_MAC_CONTROL_REG_k register, and other functions and macros are defined to access the Enet registers, but they seem to be unused and seem to be instead accessed via the IOCTL interface.
How to set the EXT_EN bit in the CPSW_PN_MAC_CONTROL_REG_k register via the IOCTL interface?
It seems that the relevant ENET registers are set in EnetApp_driverOpen().
Can "CSL_CPGMAC_SL_enableExtControl()" be added after EnetApp_driverOpen()?
Best regards,
Daisuke
Hi Shaunak-san,
Thank you for your support. Our customer is waiting for your reply.
Please give me an answer as soon as possible. Your prompt reply would be appreciated.
Best regards,
Daisuke
Hi Shaunak-san,
Sorry for many times. Our customer is waiting for your reply.
Please give me an answer as soon as possible. Your prompt reply would be appreciated.
Best regards,
Daisuke
Hi Daisuke,
You may call it after EnetApp_driverOpen(), however calling there does not seems a good idea from software point of view,
Our suggestion is to modify in the below function in driver source code.
File :'source/networking/enet/core/src/mod/cpsw_macport.c':
static int32_t CpswMacPort_setInterface(CSL_Xge_cpswRegs *regs, Enet_MacPort macPort, const EnetMacPort_Interface *mii) { .... else if (EnetMacPort_isRgmii(mii)) { - CSL_FINS(macControl, XGE_CPSW_PN_MAC_CONTROL_REG_EXT_EN, 0U); + CSL_FINS(macControl, XGE_CPSW_PN_MAC_CONTROL_REG_EXT_EN, 1U); CSL_FINS(macControl, XGE_CPSW_PN_MAC_CONTROL_REG_GIG_FORCE, 1U); status = ENET_SOK; } ... }
After the above change, you have to clean & recompile the libraries:
gmake -s DEVICE:=am243x PROFILE:=release libs-clean gmake -s DEVICE:=am243x PROFILE:=release libs gmake -s DEVICE:=am243x PROFILE:=debug libs-clean gmake -s DEVICE:=am243x PROFILE:=debug libs-clean
Then recompile your application / project along with the changes done in "EnetApp_initLinkArgs" function to set link speed as 10mbps-
Thanks and regards,
Pradeep
Hi Pradeep-san,
Thank you for your reply.
I modified the code, built the library and example below, and ran it on EVM, but it still links up at 1-Gbps.
C:\ti\mcu_plus_sdk_am243x_09_00_00_35\examples\networking\enet_layer2_cpsw
After running it, the EXT_EN bit in the CPSW_PN_MAC_CONTROL_REG_0 register (0802 2330h) was set to 1b.
Additionally, I cleared the GIG_FORCE bit in the CPSW_PN_MAC_CONTROL_REG_0 register (0802 2330h) to 0b, but it still links up at 1-Gbps.
Have your proposed modifications been tested?
What other modifications are needed for it to link at 10M-bps?
Best regards,
Daisuke
Hi Pradeep-san,
I suspect that the PHY (DP83867) is still set to 1-Gbps.
Does the change below also force the PHY side to 10-Mbps?
linkCfg->speed = ENET_SPEED_10MBIT;
If no, how to modify to force the PHY to 10-Mbps?
Best regards,
Daisuke
Hi Pradeep-san,
Sorry for many times. Our customer is waiting for your reply.
To link up the DP83867 at 10-Mbps, the bits in the following registers will need to be set.
ANAR[8].TX_FD = 0b: 100BASE-TX Full Duplex not supported
ANAR[7].TX = 0b: 100BASE-TX not supported
ANAR[6].10_FD = 1b: 10BASE-Te Full Duplex is supported by the local device
ANAR[5].10BASETe_EN = 1b: 10BASE-Te is supported by the local device.
CFG1[9].1000BASE-T FULL DUPLEX = 0b: Do not advertise 1000Base-T Full Duplex ability
CFG1[8].1000BASE-T HALF DUPLEX = 0b: Do not advertise 1000Base-T Half Duplex ability
DP83867IR/CR Robust, High Immunity 10/100/1000 Ethernet Physical Layer Transceiver datasheet (Rev. G)
Table 8-13. Auto-Negotiation Advertisement Register (ANAR), Address 0x0004 (Page 63)
Table 8-18. Configuration Register 1 (CFG1), Address 0x0009 (Page 69)
How to modify the code to set the PHY registers?
The codes below seems to be used to set the PHY registers, but I cannot find it to modify.
C:\ti\mcu_plus_sdk_am243x_09_00_00_35\source\networking\enet\core\src\phy\
dp83867.c
enetphy.c
Please give me an answer as soon as possible. Your prompt reply would be appreciated.
Best regards,
Daisuke
Hi Daisuke,
About this
Does the change below also force the PHY side to 10-Mbps?
linkCfg->speed = ENET_SPEED_10MBIT;
Yes, it does.
Does your PHY support In-band signaling mode? The same solution is suggested to another customer and it has worked, more details - https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1292683/am243x-cpsw-10mbps-packet-transmission-error
The codes below seems to be used to set the PHY registers, but I cannot find it to modify.
C:\ti\mcu_plus_sdk_am243x_09_00_00_35\source\networking\enet\core\src\phy\
dp83867.c
enetphy.cPlease give me an answer as soon as possible. Your prompt reply would be appreciated.
Thanks for your patience! I will recreate this today and let you know more details in a day.
With regards,
Pradeep
Hi Pradeep-san,
Thank you for your reply.
Does your PHY support In-band signaling mode? The same solution is suggested to another customer and it has worked, more details - https://e2e.ti.com/support/microcontrollers/arm-based-microcontrollers-group/arm-based-microcontrollers/f/arm-based-microcontrollers-forum/1292683/am243x-cpsw-10mbps-packet-transmission-error
I guess they are testing with a 10-Mbps link partner.
Thanks for your patience! I will recreate this today and let you know more details in a day.
Thank you for your kindly support!
Please give me an answer as soon as possible. Your prompt reply would be appreciated.
Best regards,
Daisuke
Hi Daisuke,
I have gone through your logs, and able to recreate the scenario in our tests.
To set the link speed manually, in in-band operation, we need to manually configure the link speed and link duplexity to required values in the application.
Setting either link speed or link duplexity to 'AUTO' will result in advertising capabilities of 100M and 1G, along with 10M. We will fix it separately. However, would suggest you NOT to set both speed and duplexity to AUTO for now.
Please set the following configuration in the application and driver source code to enable 10-Mbps in in-band mode:
File :'source/networking/enet/core/src/mod/cpsw_macport.c':
static int32_t CpswMacPort_setInterface(CSL_Xge_cpswRegs *regs, Enet_MacPort macPort, const EnetMacPort_Interface *mii) { .... else if (EnetMacPort_isRgmii(mii)) { - CSL_FINS(macControl, XGE_CPSW_PN_MAC_CONTROL_REG_EXT_EN, 0U); + CSL_FINS(macControl, XGE_CPSW_PN_MAC_CONTROL_REG_EXT_EN, 1U); CSL_FINS(macControl, XGE_CPSW_PN_MAC_CONTROL_REG_GIG_FORCE, 1U); status = ENET_SOK; } ... }
After the above change, you have to clean & recompile the libraries:
gmake -s DEVICE:=am243x PROFILE:=release libs-clean gmake -s DEVICE:=am243x PROFILE:=release libs gmake -s DEVICE:=am243x PROFILE:=debug libs-clean gmake -s DEVICE:=am243x PROFILE:=debug libs
Then recompile your application / project along with the changes done in "EnetApp_initLinkArgs" function to set link speed as ENET_SPEED_10MBIT (10mbps) and Link duplexity as ENET_DUPLEX_FULL -
Please let us know if you face any further issues regarding this topic.
Thanks and Regards,
Teja.