This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello,
Followed instructions in "C:\ti\Hercules\HALCoGen\v04.07.01\examples\TMS570LC43x\example_rtiBlinky.c" to have created the HALCoGen project and the corresponding CCS project. However, when the built project image is running on the LAUNCHXL2-570LC43 eval board, no LED blinking was observed at all.
Please advise. Thank you.
Hi Jagadish,
Thank you for the reply. Please refer to the attached CCS project, which I created by following the instructions in "C:\ti\Hercules\HALCoGen\v04.07.01\examples\TMS570LC43x\example_rtiBlinky.c", and also tested it on our LAUNCHXL2-570LC43 eval board, but observed no blinking LED at all.
When following the instructions in the example_rtiBlinky.c, I noticed that there is no mentioning of any GIO configuration. Is this expected? If so, then how will the LEDs at GIOB_6 or GIOB_7 (per the eval board schematic) be driven to blink?
I also checked the TMS570LC4357 tutorial that you showed in another thread, but, the tutorial is for using another entirely different eval board from TI. Thank you and I look forward to your reply.
One more note, Jagadish: I also commented out the function definition/declaration of rtiNotification in "...source\HL_notification.c", and then build the project and test it on our LAUNCHXL2-570LC43 eval board, but still, no blinking LED was observed at all. Thanks.
Hi Jagadish,
I was able to revise the TI sample code in "C:\ti\Hercules\HALCoGen\v04.07.01\examples\TMS570LC43x\example_rtiBlinky.c", and now have software that can run on the TMS570LC43 eval board, to blink the two user green LEDs. The revised HL_sys_main.c is attached.
I am also wondering: So, for which TI eval board, was the source code in "C:\ti\Hercules\HALCoGen\v04.07.01\examples\TMS570LC43x" developed for?
Please advise. Thanks!
/** @file HL_sys_main.c * @brief Application main file * @date 11-Dec-2018 * @version 04.07.01 * * This file contains an empty main function, * which can be used for the application. */ /* * Copyright (C) 2009-2018 Texas Instruments Incorporated - www.ti.com * * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ /* USER CODE BEGIN (0) */ /* USER CODE END */ /* Include Files */ #include "HL_sys_common.h" /* USER CODE BEGIN (1) */ #include "HL_system.h" #include "HL_sys_core.h" #include "HL_mibspi.h" #include "HL_esm.h" #include "HL_rti.h" #include "HL_gio.h" #include "HL_het.h" /* USER CODE END */ /** @fn void main(void) * @brief Application main function * @note This function is empty by default. * * This function is called after startup. * The user can use this function to implement the application. */ /* USER CODE BEGIN (2) */ /* USER CODE END */ int main(void) { /* USER CODE BEGIN (3) */ /* Initialize RTI driver */ systemInit(); gioInit(); rtiInit(); /* Set high end timer GIO port hetPort pin direction to all output */ // gioSetDirection(hetPORT1, 0xFFFFFFFF); /* Enable RTI Compare 0 interrupt notification */ rtiEnableNotification(rtiREG1,rtiNOTIFICATION_COMPARE0); /* Enable IRQ - Clear I flag in CPS register */ /* Note: This is usually done by the OS or in an svc dispatcher */ _enable_IRQ_interrupt_(); /* Start RTI Counter Block 0 */ rtiStartCounter(rtiREG1,rtiCOUNTER_BLOCK0); /* Run forever */ while(1); /* USER CODE END */ } /* USER CODE BEGIN (4) */ /* Note-You need to remove rtiNotification from notification.c to avoid redefinition */ void rtiNotification(rtiBASE_t *rtiREG, uint32 notification) { /* enter user code between the USER CODE BEGIN and USER CODE END. */ /* Toggle HET pin 0 */ // gioSetPort(hetPORT1, gioGetPort(hetPORT1) ^ 0x00000001); /* Toggle GIOB6 and GIOB7 for user green LEDs 1 and 2 on TMS570LC43 eval board*/ gioSetBit(gioPORTB, 6, gioGetBit(gioPORTB, 6) ^ 0x00000001); gioSetBit(gioPORTB, 7, gioGetBit(gioPORTB, 7) ^ 0x00000001); } /* USER CODE END */