Part Number: LP-AM243
Tool/software:
I have an application with two tasks that I would like scheduled by a RTOS, ideally dynamically leveraging all four cores on the LP-AM243x. This thread is two years old and I was wondering if anything had changed regarding support for SMP?
For background one task is responsible for gathering data from the dev board pins and buffering it in a FIFO queue and the second task is responsible for pulling data from the FIFO queue, processing it, and either: 1) sending it out over ethernet, or 2) buffering it to be sent by a separate task (COA still TBD).
If there still isn't support for SMP on the LP-AM243x via FreeRTOS, what is the best way to have two tasks running on separate cores with a shared FIFO queue?
Any examples to support the response are appreciated.
Thanks in advance,
Brian