This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
In my SRAM address parity test RAMERRSTATUS is set for both B1 and B2 as expected when I inject parity error, but there is no ESF10 and ESF12 bits set in the ESMSR1. I do esmInit() on startup. Is there anything else I need to do to allow this error to be flagged to the ESM? Do I need to do anything with the VIM for this?