This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I brought MSP-FET (black color). This is the newer version of MSP-FETUIF from TI. when I am trying to use it, gives "MSP430: Error initializing emulator: No USB FET was found" error. So far I used MSP430G2553LP as debugger via Spy-Bi wire without any issues. Is MSP-FET need any configuration is CCS or any drivers to be installed in Windows ?
My usage environment :
1. Windows-7 64 bits.
2. CCS Version: 5.5.0.00077
3. Target MSP430F5338.
I appreciate any help.
Thanks.
Thanks for reply.
Sorry, I was busy in other activity and could not see/respond soon.
Yes, I see drivers installed (application and debug) in device manager.
Any help is appreciated.
Thanks.
Hi Jens-Michael,
Thanks a lot for your reply.
I am unable to find out how CCS is configured to COM port to be used. I did check debug config in CCS5.5 but could not find it. I guess, CCS configures itself to available COM port and uses it.
I checked in Windows device manager and seems okay. It is using COM11 and COM12. I have attached the screen shot.
It works well with Elprotronic FET-Pro430. I could access MSP430-F5338, read/write memory etc. msp-fet.docx
I read few e2e threads but non-explained about this issue. I read one thread and it says, only CCS6 supports this tool. I am not sure if this is the case. We are using CCS5.5 and we would like to continue as our project is at the end of development stage and we do not want to move to CCS6 just to use this tool.
Any help is appreciated.
Regards,
CB Kolar
TI support,
We are still waiting on an answer to this question of downgrading firmware in the MSP-FET pod, so it will work with CCS v5.
Thanks Steven,
TI should have provided this information in the product description. I have purchased this product 2+ months back and wasted lot of time.
CCS5 will work with the new MSP-FET. These are the steps:
1. Go to this website: http://www.ti.com/tool/msp430-flasher?DCMP=MSP430&HQS=Other+OT+msp430flasher
2. Install MSP-Flasher-Windows
3. Once downloaded, open this directory on your PC: ccsv5\ccs_base\DebugServer\drivers
4. Open the newly installed MSP-Flasher-Windows zip; Copy “MSP430.dll”, and replace the “MSP430.dll” instance that’s in the directory from step 3.
Restart CCS and it should work.
Please click Verify Answer if this solved your problem.
Hi Lina,
Thanks for the response. I updated MSP430.dll as you explained above. But, now I get "Error connecting to the target: Unknown device" ERROR. I did re-start CCS and my laptop 2-3 times, no help. How can I fix this issue and use MSP-FET ?
Regards,
CB Kolar
Hi CB,
Reference this E2E post: http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/179058
Have you checked your programming cable?
Hi Lina,
Thanks.
1. I did go through the link you sent. But, no help.
2. I used the same MSP-FET and cable through Elptronic FET-Pro430 and it works.
3. When I tried to connect MSP-430 to target using CCS5.5, I get "Error connecting to the target: Unknown device" ERROR message.
4. Currently I am using LP (Spy-Bi wire) as debugger along with CCS5.5 without any issue.
I brought MSP-FET for better speed but unfortunately does not work.
Regards,
CB Kolar
Hi CB,
Thanks for the additional info. The error you describe is caused by the JTAG knowing that it sees the device, but not receiving the correct information from it to proceed.
How long is your programming cable?
Reference pg.24/25 of this document: http://www.ti.com/lit/pdf/slau278
Note the 2.2nF capacitor. This is used to eliminate noise in regards to the reset line. However, if using a larger programming cable than recommended, parasitic capacitance in the cable + the 2.2nF capacitor cause an excessive delay in the communications, which could result in the exact error you are seeing. A way to combat this is to use a smaller capacitance value, somewhere around ~1.1nF (See Note B). This amount would still resist noise, but would also refrain from affecting the communications. What size capacitor are you using?
Let me know if this helps.
Hi Lina,
Thanks for your reply. Sorry, I was on vacation and could not see/reply.
1. The capacitor value is 2.2nF.
2. I am using the cable supplied with the MSP-FET which is 3 feet long.
3. After seeing this message, I tried with another USB cable which is 1.5 feet long. But, no use, I am getting same error message as above.
I need it to make it work with CCS5.5. Any help is appreciated.
Regards,
CB Kolar
I had problems getting the new MSP-FET to work on Rowley compiler v3.0.0. PC on Win7
Turned off the AVG Security Software
Downloaded MSPDS-USB-Drivers onto a
NEW Win XP (Avoiding all Windows Automatic Updates and can still use my old Mechanical drawing & Graphic Packages) Machine running an old Browser.
Black Box MSP-FET worked first time
Transferred MSPDS-USB-Drivers to the WIN7 PC Machine
Initialised the MSP430 License to the MAC Addr
Hey Presto Ran Tickety Boo
I am a PDE (Product Design Engineer) not a PC Expert.
I only design Embedded Systems/Products at 63 yrs old never been so busy.
Hoped this helps.
Ian
**Attention** This is a public forum