This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
Tool/software: TI-RTOS
Hai,
I am currently working on MSP432 launchpad. Can I use 24 Mhz crystal instead of 48Mhz ?
Is there any guide available for fixing the baud rate of UARTs?
Regards,
Tom Victor
tom victor said:I am currently working on MSP432 launchpad. Can I use 24 Mhz crystal instead of 48Mhz ?
Yes you can. Why you would want to change crystal if 48MHz works?
tom victor said:Is there any guide available for fixing the baud rate of UARTs?
Sure. Baud rate generator of UART is very flexible. You shall read msp432 Users Guide (slau356), chapter "22.3.10 Setting a Baud Rate" and "Table 22-5. Recommended Settings for Typical Crystals and Baudrates"
**Attention** This is a public forum