Part Number: MSP430F6779
Hello,
As the workaround of SD3 which is the errata of SD24_B, is there any problem with the following idea?
When "-VFS" is input to SD24_B, if it is set to 2's complement, it will not be the value described in the manual.
However, its output value may be treated as a minimum value.
Or
It is an illegal value and can not be used at all.
(In that case, is it a fixed value?)
Regards,
Da