This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
As the workaround of SD3 which is the errata of SD24_B, is there any problem with the following idea?
When "-VFS" is input to SD24_B, if it is set to 2's complement, it will not be the value described in the manual.
However, its output value may be treated as a minimum value.
Or
It is an illegal value and can not be used at all.
(In that case, is it a fixed value?)
Regards,
Da
Hello,
What gain are you using? If it's set to 1, then you may have to modify your external passives (e.g. burden resistor) to reduce the max amplitude of the input signal. If you're using a gain higher than 1, you could reduce your gain to ensure that the amplitude of your input signal never exceeds +/-FS.
If you're reaching -FS during testing only and your input signal will never reach -FS, then I wouldn't worry about this issue.
Regards,
James
MSP Customer Applications
Hello,
Yes, you're correct. The input range must not exceed -VFS. If I've answered your question, please click the green "This Resolved My Issue" button.
Regards,
James
MSP Customer Applications
We have a request from the customer and ask you a question.
Is there a way to avoid this phenomenon using software other than Gain setting and 2's complement?
In the customer's environment, it is not possible to limit the input range by the gain control.
In this state, they want to know how to deal with "- VFS" input.
In the range confirmed by the customer's environment, it becomes 0xF7FFFFFF at the input of "- VFS".
Which individuals will be 0xF7FFFFFF?
When "0xF7FFFFFF" is output as AD conversion data, please tell me how to deal with software.
Regards,
Da
**Attention** This is a public forum