This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I had a question on this note from SLAU647 (rev N), in table 15, it states that the backchannel UART with flow control is only available on Rev 1.2 of the EZ-FET debugger:
Does this mean that backchannel UART flow control is not available on the MSP-EXP430G2ET Launchpad since it looks like this Launchpad uses the rev 2.0 EZ-FET?
Regards,
Munan
Hi Dennis,
So it seems that the RTS and CTS signals as they appear on the EZ-FET portion of the G2 Launchpad schematic is not pinned out on the G2 Launchpad. These pads in the gerber are NC.
But if the customer was to somehow bluewire them to some IOs on the G2 target device socket, would the UART hardware flow control work? Or is the firmware specific to which hardware revision it is?
Regards,
Munan
Hi Munan,
Sorry for the delay in my response.
My understanding is the IO pins designated as CTS and RTS are just general purpose IO pins controlled via software, not the UART peripheral. On those launchpads that don't have these connections routed to the jumper block, yes, a user can make those connections manually. But to emphasize, the software must explicity drive these during the exchange with the ez-FET.
**Attention** This is a public forum