Other Parts Discussed in Thread: AM3517, AM3505, OMAP-L137,
Hello,
I am working with a TPS65910A3A1, struggling to enable output. When power is applied I get a 1.8V on VRTC but the rest of the output rails will not turn on. I believe it is configured to start when power is applied which is how I intend it to work.
It is configured as follows:
BOOT0 = GND
BOOT1 = VRTC
PWRHOLD = Pull up to VRTC through 10K resistor. (Tried pulling LOW and leaving floating)
PWRON = Pull up to VRTC through 10K resistor. (Tried pulling LOW and leaving floating)
SLEEP = GND
BACKUP = +5V Input Voltage (Tried floating)
Schematic is attached.
Please note:
- the 3.3V input source on VDDIO (pin12) is enabled by VAUX33 (pin4) output.
- R16 is not populated
- TP1-TP11 are not connected ( floating)
- I tried grounding pin 31, SW3 per schematic checklist since VDD3 is not used.
- There are 2.2uF capacitors on VDIG1, VDIG2, VAUX, VAUX33, VDAC18, VRTC (not shown)
- I am testing without load.

Thank you.