This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
if insertion or removal of battery packs test, then Our customer product have BTST 10R/REGN Schottky/Low side MOSFET damage issue,
is this issue Related CE sequence? Our customer CE is link to detect BATTERY.
Hi Sir,
The damage have BQ24610 Pin18 & Pin19 short, BTST 10R=1K(damage), REGN Schottky=short(damage), Low side(damage)
Battery plug in Vout max is ADP in 19V.
we are see the TI BQ24610EVM REGN Schottky is used the ZLLS350 Continuous Forward current 380mA,
But customer is D4=RB751V(M)-40(TE17)/SOD-323 Average rectified Forward current 30mA, is the level too small damage D4?