We are considering the configuration shown in the diagram for AM6254.
The GigabitPHY IC(DP83867) is connected via RGMII1, while the 100M PHY IC is connected via RMII2.
Can we use both RGMII and RMII with CPSW?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We are considering the configuration shown in the diagram for AM6254.
The GigabitPHY IC(DP83867) is connected via RGMII1, while the 100M PHY IC is connected via RMII2.
Can we use both RGMII and RMII with CPSW?

Hello user3895290
Thank you for the query
https://www.ti.com/lit/ml/sprad05/sprad05.pdf
7.3 Ethernet Interface Using CPSW3G Common Platform Ethernet Switch 3-port Gigabit Ethernet
The CPSW3G interface can either be configured as a three port switch or a dual MAC interface. Both interfaces can have their own MAC address.
CPSW3G support RMII (10/100) or RGMII (10/100/1000). For RMII interface, see the CPSW0 RMII Interface section of the device-specific TRM for the recommended configuration.
CPSW3G allows using mixed RMII/RGMII topology.
The below FAQ provides link to the key collaterals that could be used including the TRM.
Regards,
Sreenivasa