This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, TI engineers.
I design RMII interface circuit.
I will route the source from external 50MHz crystal oscillator to the MPU and 2 PHY chips.
In TRM, I am confused about the description of RMII_REF_CLK connection.
When using external clock source, other interface pins of RMII is indicated "n", n is 1 to 2, for example RMII"n"_TX_EN means RMII1_TX_EN and RMII2_TX_EN pin.
However, there is no "n" for RMII_REF_CLK.
In datasheet, RMII1_REF_CLK(pin AA16) & RMII2_REF_CLK(pin AA20) is surely noted.
1) Is this meaning that only one routing to Pin AA16 or Pin AA20 is OK except routing to PHY chips?
2) Or should I route both Pin AA16 & AA20 and 2 PHY chips?
In case of 1), I might need 3-output clock buffer(LMK1C1103).
Otherwise, for case 2), I have to use 4-output clock buffer(LMK1C1104).
And also, I want to know what the length of each routing path has to be.
Regard.
Hello HOGYUN RYU
Thank you for the query and the analysis
1) Is this meaning that only one routing to Pin AA16 or Pin AA20 is OK except routing to PHY chips?
2) Or should I route both Pin AA16 & AA20 and 2 PHY chips?
You need to connect clock to both pins
In case of 1), I might need 3-output clock buffer(LMK1C1103).
Otherwise, for case 2), I have to use 4-output clock buffer(LMK1C1104).
it is recommended to us a dual output buffers for design flexibility.
And also, I want to know what the length of each routing path has to be.
Do you have a length of the length you are considering?
Regards,
Sreenivasa
Thanks for your answer.
First of all, there was some mistake to express.
The meaning of the routing length is that each routing path has to be the same length. In my case, the four path of routing length (from a clock buffer to 2 refference clock input pin of AM62A7(AA16 & AA20) and 2 PHY chips) should be the same?
Secondly, what do you mean you recommend using dual output buffer?
I have already mentioned 3-channel and 4-channel clock out buffer IC.
Could you specify a model that you said as "dual output buffers"?
And I want you to explain about "design flexibility" in detail, if you don't mind.
Finally, I draw a simple schematic what I will design through your answer.
Is this correct?
I will wait for your reply.
Regard
Hello HOGYUN RYU
Thank you.
Please review the below checklist for ethernet interface.
https://www.ti.com/lit/an/sprad21e/sprad21e.pdf
The recommendation is to use 2 X dual buffer , one for each EPHY for design flexibility.
The Diagram looks good if the routing is manageable. Alternatively as mentioned above using 2 X dual clock buffer can be considered.
Regards,
Sreenivasa