This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir:
I see in document SPRABL1A (DDR3 Design Requirements for KeyStone Devices Application Report) page 72,
CS1# is described in table 40 as "Leave unconnected" for two rank design, is it right?
what is more, we have a design based on C6678 and we want to achieve most as large DDR3 storage capacity as possible,
and 2 ranks design should be used. I think we should use 16 pieces of X8 DDR3 device should be used, is it right?
The 8 pieces in rank0 is the same with the 8 pieces in rank1 in pin connection except for the first 8 pieces connected to
CS0# and the other 8 connected to CS1#, is it right?
Thank you very much.
You are correct that CS1# would be connected to eight of your devices in a dual rank design. The error in the table on page 72 will be corrected in the next release. Please be sure to follow all the routing guidelines carefully. Dual rank systems are difficult to route due to the stub length requirements. Also note that the address mirroring used on some DIMMs to shorten stubs on the address lines is not supported by the C6678.
Thank you Bill.
Does C6678 support RDIMM usage? Only UDIMM is mensioned in C6678 DDR3 design documentation.
Hi Sir
We have a problem,Our customers need 8G memory for C6678,we use 10 pieces (contain ECC)of MT41K512M16HA-125 IT and fly-by for layout,
Five pieces SDRAM on top,Five pieces SDRAM on bot,dual rank,Can this be designed?
we found,memory will go wrong t when the CS0 、CS1 is turned on by software, But when turn off the CS1, the memory will not go wrong,
How do we solve this problem?thanks!
This should have been set up as a totally new thread with a proper title. That way others can search for the feedback. Please start a new thread and we will respond to it.
BTW, I am sure this is answered already in another forum post.
Tom
The KeyStone I DDR3 Initialization Application Report (SPRABL2D) was revised in January of 2015. It now contains instructions for configuring the Controller and PHY to support twin-die SDRAMs. This was not validated on any TI reference design but we provided this guidance as a service to customers eager to try it. Based on feedback from those who implemented this, we believe that this configuration is valid. However, we do not have confirmation that this was ever implemented on a board that went to production. There were reports that some boards that implemented twin-die devices had layout issues resulting in occasional errors. More recently monolithic 8Gb DDR3 SDRAM devices became affordable and we have not seen interest in twin-die use since then. As stated previously, we believe that the guidance provided is sufficient for success but we cannot guarantee it since we did not characterize it on a TI reference platform. Therefore, our current recommendation is to implement DDR3 SDRAM topologies using monolithic (single-die) SDRAMs.
Tom