This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey,
We are using theTMS320C6748. The datasheet says that USB0_VDDA12 must be connected to a 0.22uF capacitor - table 3.32 in the datasheet.
However the checklist here says that if both USB ports are not used then the pin should be a no connect - http://processors.wiki.ti.com/index.php/OMAP-L13x_/_C674x_/_AM1x_Schematic_Review_Checklist#USB
This is an avionics design that was done year or two ago and the original datasheet said to leave the pins unconnected. We are finishing verification and have just seen the updated datasheet.
Can you tell me if the datasheet is correct or the checklist?
Cheers
Calum
Hi Calum,
For TMS320C6748, do you want to use the USB ports, USB0 or USB1 or both USB0 & USB1 or none of the USB ports ?