I updated the EVM board (Rev D, Micron) with the images in the above mentioned SDK (which is as far as I know the newest).
While booting from flash I get several messages (see below) What might be wrong here? (What I found is OneNand instead of used NAND (Micron)). But this is probably not all the reason. Howto change?
Thanks
------------------------
regulator: VUSB1V8: 1800 mV normal standby
twl_reg twl_reg.18: can't register VUSB1V8, -16
twl_reg: probe of twl_reg.18 failed with error -16
i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
OneNAND driver initializing
omap2-onenand omap2-onenand: Cannot request GPMC CS
omap2-onenand: probe of omap2-onenand failed with error -16
Power Management for TI OMAP3.
Division by zero in kernel.
[<c0039524>] (unwind_backtrace+0x0/0xdc) from [<c018027c>] (Ldiv0+0x8/0x10)
Division by zero in kernel.
[<c0039524>] (unwind_backtrace+0x0/0xdc) from [<c018027c>] (Ldiv0+0x8/0x10)
SmartReflex driver initialized
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
tvp514x 3-005d: chip id mismatch msb:0xfb lsb:0xfb
tvp514x 3-005d: Unable to detect decoder
omapdss DPI error: display already enabled
omap_vout omap_vout: 'lcd' Display already enabled
dev: starting version 141
udevd[531]: inotify_add_watch(3, (null), 10) failed: Bad address
...
Remounting root file system...
WARNING: Couldn't open directory /lib/modules/2.6.32: No such file or directory
FATAL: Could not open /lib/modules/2.6.32/modules.dep.temp for writing: No such file or directory
modprobe: FATAL: Could not load /lib/modules/2.6.32/modules.dep: No such file or directory
modprobe: FATAL: Could not load /lib/modules/2.6.32/modules.dep: No such file or directory
root: mount: mounting rootfs on / failed: No such file or directory
root: mount: mounting usbfs on /proc/bus/usb failed: No such file or directory
Setting up IP spoofing protection: rp_filter.
Configuring network interfaces... done.
Wed Dec 2 19:19:00 UTC 2009
INIT: Entering runlevel: 5
Starting telnet daemon.
modprobe: FATAL: Could not load /lib/modules/2.6.32/modules.dep: No such file or directory
Starting syslogd/klogd: done
Starting thttpd.
Starting OMAP Demo application.