This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Comparing Devices
[FAQ] OPT3004: OPT3001 vs OPT3004, what is the difference?
[FAQ] OPT3001: OPT3001 vs OPT3002
Optics
[FAQ] OPT3001: What is the f1' value of the OPT3001?
Electrical
Software
[FAQ] OPT300X Family Parts: What are the available drivers for TI's family of ambient light sensors?
[FAQ] OPT3001: Is there example raspberry pi code for the OPT3001?
[FAQ] OPT3001: Do Linux/Android drivers exist for the OPT3001?
[FAQ] OPT3001: Is there MSP430 code for use with the OPT3001?
Mechanical/Assembly
ALS OPT300x Handling Instructions
[FAQ] OPT3001: Where is the STEP model (.STP) for the OPT3001?
Performance/Accuracy
[FAQ] OPT3001: What is the performance under flickering LED Light
[FAQ] OPT3001: What is the accuracy of an OPT300x part?
[FAQ] OPT3001: Why does the OPT3001 not have any data taken outside, under sunlight?
[FAQ] OPT3001: Why does the OPT3001 not have a range that measures full sunlight at 130Klux?
EVM
[FAQ] OPT3001: Are the OPT3001EVM PCB files available?
[FAQ] OPT3001: Debugging connection issues with the OPT3001EVM