This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I've bought TMS320C6678 EVM. CCS version came with the board was CCSv5.0.23. Since it had a number of bugs, I was forced to download CCSv5.1.
I have the CCSv5.0.23 license and I want to license CCSv5.1. How can I do that? or How can i get a license for CCSv5.1?
Regards,
Sohal
HI Mohamed,
CCSv5.1, as it is a full production release is licensed differently to the beta versions (which is what 5.0.xx was) and does not work with a v4 license.
You have a few options
1 - if you have a v4 license with an active subscription, you can upgrade your license to a v5 one
www.ti.com/myregisteredsoftware
2 - You can use on the free license options (for example CCSv5.1 is free to use with the XDS100 and certain mezzanine cards on certain EVMs)
3 - you can purchase a v5 license.
This wiki has further details and describes these license options and more.
http://processors.wiki.ti.com/index.php/Licensing_-_CCS
Best Regards,
Lisa